I bought a couple of the UCB-A and USB-C host versions of the https://www.sparkfun.com/products/21271 “SparkFun 4-in-1 Multi-USB Cable - USB-C Host” cables.
With two different USB-C wall warts the USB-C connector on the “hydra” wasn’t putting out enough Voltage to start an attached device charging.
I put a device on there that reports the input Voltage and it said the hydra was sending out only 3.9V and 1.1 Amps. When I used a “plain vanilla” USB-C cable between that same wallwart and the measuring device and it reports 4.194 Volts at 1.45 Amps.
So it seems like this cable has enough of a Voltage drop across it that it doesn’t function as a charging cable? Anybody else seeing this?