I am creating a device that can measure scalp oximetry, scalp temperature and EEG. I have the OpenBCI Cyton board for the EEG. I am planning on purchasing the MAX30105 to do the oximetry and temperature. I was wondering if I could use the Cyton board to communicate with the MAX30105, or do I need to get another microcontroller? The Cyton board has the PIC32MX250F128B microcontroller.