Mounting Dimensions of Sparkfun Redboard Artemis ATP

Hello,

I am looking for a Dimensional drawing of the Sparkfun Redboard Artemis ATP.

Specifically, I would like to know where the 4 mounting holes are at (see image attached).

If seems the holes are for an M3 screw. It would be helpful to list the dimensional drawings on the product page on sparkfun along with the size of the mounting holes. I see them for other products but not for this one.

The hardware files are on github, but I do not have the eagle program to be able to view them and take measurements.

Thank you,

-manuel

You can always try to free BRD viewer online e.g. https://www.altium.com/viewer/ to upload a BRD online.

A bit more information might help you. Looking at your picture.

The external size of the ATP is 590mm x 1018mm

The holes are 3.3mm (thus M3)

The center of the holes you indicated are all 5.0mm from the long sides.

Hole_1: The center hole top left: is 92 mm from the right hand

Hole_2: The center hole top right: 15 mm from the right hand

Hole_3: The center hole bottom left: is 965mm from the right hand

Hole_4: The center hole bottom right: is 14mm from the right hand

hope that helps.

Thank you Paul, I didn’t know about the altium viewer. I will continue using that for gathering future dimensions.

Hi,

I think the Altium Viewer must have confused inches and mm in some way? Or perhaps cm and mm? Maybe there is a setting that can be changed.

I’ve attached the dimensions from Eagle. The units are inches. I hope this helps.

Best wishes,

Paul