I’m trying to find an easy way to lift a TSSOP part off of a production board and replace it with a part that would have a straight pass thru on 5 of the data lines. Unfortunately we don’t want to use this TSSOP voltage leveler and need it to just pass thru 3.3V signals directly.
Is anyone aware of a straight pass thru for TSSOP parts that would simplify the rework? Yes, we should have caught this in design, but with 60 boards out there, we can’t just start over.
You can remove TSSOPs in a few ways. The easiest is to use a hot air rework station. You heat the whole part and once the solder melts, just lift it off. If you don’t have access to a rework station, with a hobby knife or other fine tipped cutting device you can cut the pins where they enter the TSSOP package on both sides, lift the body of the part out, and then individually remove the pins from the board using a soldering iron.
You’re unlikely to find a drop in part that only passes through the specific pins you need. You will most likely have to solder tiny jumper wires in place between the correct pads for the removed part. This isn’t uncommon in the world of PCB development.
If you are OK with 10 ohms resistance, there are some TSSOP isolated resistor arrays. You didn’t mention the pinout or part size so it is difficult to give any better info.