Not Able to communicate from Arduino IDE to f9p Board

Hi ,

I was trying to run the Example3_StartRTCMBase from SparkFun_Ublox_Arduino_Library ->Example->ZedF9P .

Setup :

Sparkfun Physical Board : Zed F9P

My Arduino Version is : 1.18.13

Downloaded and installed library from: https://github.com/sparkfun/SparkFun_Ub … no_Library

Added SparkFun SAMD boards with version 1.7.7 with : https://raw.githubusercontent.com/spark … index.json

Arduino SAMD board version is : 1.8.9

In Arduino IDE I am using Board : SparkFun 9D oF Razor IMU m0

Error :

Sketch uses 40008 bytes (15%) of program storage space. Maximum is 262144 bytes.

An error occurred while uploading the sketch

No device found on COM3

Observations :

I also observed incoming NMEA messages on the same COM port

I also tried with other versions of Sparkfun SAMD : 1.8.6 and Arduino SAMD :1.7.4 . Still I find the same Error .

Please advice on how to work this out .

Thank you ,

Goutham

What microcontroller board are you using?

Otherwise, as mentioned in the [hookup guide, the USB connector on the ZEDF9P GPS module is for use with the U-Center software. See hookup guide for more details.](GPS-RTK2 Hookup Guide - SparkFun Learn)