Hi Paul,
I got the combo including the antenna, but I do not get a result.
I work with the IDE D9S Example 1 and do not get a RXM PMP message.
The combo came with the firmware 1.13 and I will update it to 1.32, but this is not the problem.-
The problem is not getting L1 signals. I can not see anything in u-center, when I go to RXM PMP.
I work outdoors with clear view to the sky in south direction.
As far, as I understand the como has to work with your code D9S Example 1. Correct?
In the example I have only changed the frequency to eu.
As I explained, I use the u-blox antenna, which you are using also.
Do you think I need an antenna with eu frequency? But the u.-blox wokrs with you ?
What is my fault?
greetings
Bernhard