Hello!
I’m having trouble getting an OpenScale board to work as expected.
With 4x 50kg loadcells connected to the built-in combinator, I get no weight reading (only 0) and the raw data from open scale is not varying.
I measured the resistance between pairs and think I figured that the red wire is indeed the center-tap.
Attached is a picture of the setup I’m using.
Am I missing something here? Is there a jumper or a configuration that needs to be made so that the board uses the combinator output instead of the screw terminal load cell?
Thanks in advance!