Hello everybody,
I just got the surveyor and I am in the process of setting up the following system for outdoor mapping:
RTK data is received by my iphone und transmitted via wlan hotspot to a microsoft surface go 2 tablet using the Ntripclient (lefebure). GPS input comes via L1/L2 antenna and the surveyor via BT in the tablet. the surveyor creates two ports, com 4 and com3. Starting the ntripclient, the gps data comes in via com3 and the rtk via iphone and the surveyor indicates RTK on the LED, so far everything looks nice. However, If I want to use my mapping software (ocad) com3 cannot be opened (because it is busy with the ntripclient, I assume) and com 4 doesn’t send any recognizable data. I also cannot use com4 for input of the GPS signal from the antenna.
To check if my mapping software is compatible with the setup, I stopped the ntrip client, and the GPS signal flows perfectly from the antenna via surveyor and BT com3 to the tablet and provides live access in my mapping software , the surveyor indicates 100cm, so this part works perfectly.
Now I just have to get the two things together to get rtk date into my mapping software? I was assuming that the second port com4 is in charge of this, but this port doesn’t send or recieve any regognizable data?
Unfortunately I cannot use android as my mapping software is windows based, so I cannot compare it with the software used in the hook up guide
Any ideas what I am doing wrong?
Thanks a lot
Stephan