pls - howto dump intel cfi flash content to file?

Hi folks

want to make binary dump of the content of my intel 16MB flash on Pronghorn IXP425 board

with command dump image

Script below does not do this and hangs

what changes should I make to get it done

Thank you for your help

#daemon configuration

telnet_port 3333

gdb_port 4444

#interface Olimex OpenOCD–[begin]

interface ft2232

ft2232_device_desc “Olimex OpenOCD JTAG TINY A”

ft2232_layout olimex-jtag

ft2232_vid_pid 0x15ba 0x0004

jtag_speed 16

jtag_ntrst_delay 200

jtag_nsrst_delay 400

reset_config srst_only

jtag_device 7 0x1 0x7f 0x7e

daemon_startup reset

#target

target xscale big reset_init 0 ixp42x

dump_image pronghorn.bin 0x50000000 0x1000000

slava:

want to make binary dump of the content of my intel 16MB flash

Succeded to get into telnet port 3333 and run the same command in debugger

it worked - though it took some time for debugger output showning each word loaded

I guess when trying this command in config file it also works but did not show any diagnostics