busonerd:
Does anyone have strong opinions for keeping it open [or for shutting it down, for that matter]?
Greetings Dave et al.,
I’m a big fan of BatchPCB, in spite of my recent frustration. I’d like it to stay.
That said, I think a fair and equitable position is for SFE to make money by running it as a business (and not a charity), and for users to understand the limitations. There has to be more than ‘cheap and slow’ for it to remain viable.
For my needs the biggest advantage is that I can do a one piece PCB for a hobby budget, with reasonable expectations of the outcome. If the next project uses the same PCB, or uses several of the same design, I can reorder.
Faster delivery would be nice, but I found that I can pace my work and do two or more concurrent projects that fill the twenty day timeframe well. I’m not in a position to use (or be tempted by) the “two for one” offers, or “get five day turns for the ten day price” that fill my email box from other PCB vendors.
What has to get better, if you decide to continue, is that customers are better informed of the work progress.
Changing the timeframe to six weeks and keeping the cost the same will not really help - it doesn’t motivate SFE (no profit incentive) and it won’t take long for users to expect three weeks once it became known that the service can support twenty day (plus or minus) delivery.
(1) Start by doubling the cost per unit area.
(2) Not limiting the size to anything less than 24 sq inches.
Which are the limit of the EAGLE standard license (4.0 x 6.0 inches), and also approximately the size of the popular Eurocard (100 x 160mm).
(3) Offer the same shipping options but without the hidden admin charge.
(4) Provide a satisfaction guarantee that any PCB not delivered within twenty days is free (or, given SFE 100% credit against further PCB Fabs). Customers need to see an incentive imposed on SFE.
My BatchPCB projects have been towards the 20 sq inch size. I can see that many hobby and student projects (for breakout boards) might be closer to two square inches, and this might have been the motivation to start BatchPCB and also add the ten dollar admin fee.
Perhaps a minimum order amount is the solution? It gives SFE the income stream to cover admin costs associated with each order. I see other PCB suppliers doing similar programs to get their desired dollars-per-invoice revenue.
I would use a BatchPCB style service at $100 min per order. That would put the responsibility and incentive on me to get the most value for the minimum billing of a hundred bucks!
In real terms that’s two casual restaurant meals for my wife and I. Or, two fill ups at the pump for my SUV. Or, a single ticket to a live musical event. Or, one more parts order from Digi-Key. All examples of what’s competing with my hobby PCB budget.
Comments Welcome!