Hi
Is it recommended to use a AC/DC-adaptor for powering up the gator:bit v2?
or is it the battery-box (4AAs) only?
The one I have in mind has these specs:
model 0520
Input: 100-240V AC
50/60Hz
Output: 5V ---- 2A
best regards
Sophie
Hi
Is it recommended to use a AC/DC-adaptor for powering up the gator:bit v2?
or is it the battery-box (4AAs) only?
The one I have in mind has these specs:
model 0520
Input: 100-240V AC
50/60Hz
Output: 5V ---- 2A
best regards
Sophie
Hello Sophie,
The recommended DC input is rated between 2.7V - 9V. Your power supply should work.
I hope this helps.
I’m deciding between getting a 4xAA battery set (https://www.sparkfun.com/products/9835) or the rechargable lithium ion battery pack (https://www.sparkfun.com/products/15204) for powering a micro:bit + the gator:bit v2. (I noticed that my 2xAAA pack doesn’t provide enough to power the gator’s speaker.)
Any advice on those?
The 4AA battery pack would be a better option, it provides more power to the gator:bit than by applying power through the micro:bit’s USB jack.
The speaker isn’t very loud on the gator:bit, but there is a switch that turns it on and off. Make sure the “Music” switch in the lower left hand corner of the board it turned on otherwise the speaker won’t work.
Double check that first, you might not need a battery after all.
I’m getting 4.8v across two of the rivets, but only a few hundred mv of meter noise across the barrel jack plug. If I plug in to the moto:bit I (thinking maybe I didn’t have good connection inside the jack to my probe), I get a steady 233mv across the pins of the jack.