Attached is an image of my schematic, and an image of the board it creates. There is no correct part for the motor I’m using (just 2 holes that wires will be soldered into) and I also have another hole for the pin that will be soldered to the microcontroller board. When I put this into board view the spot for the motor and the pin are gone. How do I fix this in the schematic view (no matching parts!)?
Thanks
EDIT: also, it looks like the resistor isn’t even drawn!
What device are you using for your motor? Is it just ‘Motor’ as text and two wires ending above and below the text? If so, that’s your problem. You need to use some kind of device with both a symbol and a footprint. Otherwise, how would Eagle know how you wanted to connect your motor? Same goes for the hole by the resistor. What happened to your resistor, I don’t know.
For this simple schematic, you might want to skip the schematic and just make a PCB drawing.
For the motor connection, just find a suitable 2-pin connector and put in the schematic. Then set the value of the connector to ‘Motor’ or whatever you want. Or if you want to learn some more about Eagle, read the tutorial, either the included tutorial or the ones on Sparkfun, and a make a device for your motor with symbol and footprint.
The resistor in your screenshot doesn’t have a footprint because it is the toplevel of resistors with the european way of showing a resistor. If you click on the right-hand arrow next to it, it will open up and show you all the various versions under it, similar to the Bourns resistor network below it. If you click on one of the resistors below R-EU, you will see that there are a lot of different resistors with various footprints.