I have QWIIC PHAT and motor driver.
What kind of 5 V Battery can power the PHAT.
This PHAT has no USB port
I want the motor running by connecting a Battery to PHAT.
Do you have a raspberry pi?
What motor driver do you have?
The kit is based on Jetson Nano
Can I use RP2040 to drive the PHAT and motor for troubleshooting.
Troubleshooting Jetson Nano is too complicated.
Can I use RP2040 to drive the PHAT and motor for troubleshooting.
You can but it would be easier to skip the phat and connect the motor driver directly to the rp2040. The phat is more for convenience when connecting qwiic devices to a pi/jetson.
Thanks. I am convinced that I need a processor like Arduino or Redboard QUIIC to really test DC motor drive. It looks like there is no technical support number to call and talk to a support engineer.
When I bought the Jetson Nano kit, it came with wrong cable. Then I bought the cable from local store.
This makes me less confident in buying more items to troubleshoot. So if somebody from Sparkfun Tech support can call me and discuss then I am ready to buy more kits