Qwiic single realy cable connectors

Hello. My son is building a model rocketry flight computer using a micro:bit and the weather:bit board. The weather:bit has an I2C port. He wants to be able to control a relay from the micro:bit so I purchased a Sparkfun Qwiic single relay.

My question is: what cable or combination of headers, etc. can I get that will allow me to connect the minuscule gnd, 3.3v, sda, and scl holes on the relay back to the port on the weather:bit? The I2C port on the weather:bit is 4 pin female. Is there something made for this? I’ve been searching and haven’t found a ready made connector. I don’t think my soldering skills are good enough to successfully solder onto the tiny holes on the single relay.

Thanks in advance for any help.

One of these will work for ya!

https://www.sparkfun.com/products/17259

Thanks. I don’t think this will work though. The single relay does not have a JST connector. It just has tiny through holes.

Is this the relay you have?

https://www.sparkfun.com/products/15093

Yes, that’s the one. I think I get it now. I was thinking the through holes marked gnd, 3.3v, sda, and scl were the only interface. But those JST ports are also input and allow for daisy chaining. Sorry, I was just confused. Thanks for your help.

No problem rabbit.

Merry Christmas!