I broke one of the DSI ports on my RPi 5. I have been looking for a way to add additional DSI ports but have been so far unsuccessful and am looking for recommendations. Thanks in advance
Camera and DSI display connectors are interchangeable, so you can have one of each, or two the same.
I guess I should have added that I needed two connectors, for both a camera and a screen.
The main way would be to buy a broken Pi 5 for parts on ebay or similar and replace via de/re-solder if the physical connector is borked and the other is in-use
It will take tools you likely don’t have and skill to remove the damaged connector and replace it without further damaging your Pi.
Just buy another Pi, the one with the bad connector can be repurposed for another application that doesn’t need both connectors.