Hello, I purchased a Raspberry Pi SSD Kit but can’t mount or use it on my Raspberry Pi 5 (rpi5) board because it is currently mounted on a Raspberry Pi 7 inch screen. The SSD Kit arrived with standoffs that have two female ends and can’t connect the SSD hat to the board and display.
Does anyone know if Sparkfun or someone sells the right size/type standoffs with a male and female end to connect to a rpi5 mounted onto the raspberry pi 7 inch screen?
I tried contacting sales and support but they directing here to ask this question.
If anyone has a link to where to purchase, it would be greatly appreciated. Below is a picture of the board mounted on the screen and the standoffs that arrived with the kit.
Thanks in advance!