RFID with OpenLog Artemis

Hi all,

I have tried to connect the SparkFun RFID Qwiic Reader to the OpenLog Artemis, but upon starting the OpenLog Artemis just says “no device detected”. I have seen that the RFID reader is not on the list of sensors recognized by Artemis OpenLog, though my question is basically whether there will be at any time an update for the OpenLog firmware that will recognize and read in data from the RFID module?

I have read the guide how to hook up the RFID reader to the Red Board, but this also requires soldering a wire between the Qwiic RedBoard’s pin 8 and the Qwiic RFID reader’s INT pin. I was hoping to connect multiple RFID readers to one Artemis via the SparkFun Qwiic 8-channel Mux, though I presume this wouldn’t work either if I have to add an additional wire from every RFID sensor to the Artemis?