ribbon cable for a 4P4C connector ?

I have a bag of 4P4C connectors, and I need to crimp a few of them onto a length of ribbon cable.

I have two kinds of ribbon cable in front of me, one is a 6-conductor/15-foot piece that I purchased from Sparkfun. The other is a 100-foot roll of very old (circa 1973) 25-conductor ribbon cable. The old stuff appears to have the correct spacing to insert into the 4P4C (caliper suggests 4+mm) while the newer cable measures 5.5mm for 4-conductors. The old cable is so old the insulation is brittle & cracking (but it’s the correct spacing). The old ribbon cable measures 25mm across 25 conductors, while the new stuff looks like 8mm across 6 conductors. So I guess I need 4mm for 4 conductors (or something with that spacing that I can cut down).

Is this readily available in 2014 ?

Yes, almost every hard wired telephone uses ribbon cable. Go to the nearest electronics/home improvement store and look for a phone extension cord. Make sure it has all 4 conductors (red green black yellow).

The 4P4C connector is the one used between the telephone and the handset. The telephone to the wall is a 6P4C (or RJ-11). Pretty much all of the handset cables I have ever seen are coiled. I need a flat ribbon, not a coiled cable. Although it may be that the cable used in the 6P4C is the same pitch I need.

I found a technical drawing that shows the pitch on the 4P4C connector to be 1.02mm (0.040 inch). That explains why the ~1.0mm pitch (ancient) cable looks so close. The smallest I’ve located thus far, is some new/old stock 3M cable at 1.08mm. Still looking.

How long must it be ? For the few pennies extra, you might buy one w/connectors and snip one end off and recrimp to get a custom length or pinout.

http://www.homedepot.com/p/Steren-25-ft … /205317853

Mee_n_Mac:
How long must it be ? For the few pennies extra, you might buy one w/connectors and snip one end off and recrimp to get a custom length or pinout.

http://www.homedepot.com/p/Steren-25-ft … /205317853

That is effectively what I did last night. In my wire box, I found a 15-ft length with RJ11 on both ends, snipped off one end, and used a about a foot of that. That worked. But the wire used in modular telephone cables is different from the wire used in ribbon cables. The difference is not merely the gauge, but there is something in the wire strands (looks like a thin vinyl strand) that is there to assist in the constant flexing that the average ribbon cable could not deal with.

The wire type I need would not have to flex as either telephone cord might, but only rarely (like a ribbon cable). I am going to give this a try, but I have no clue what the current carrying ability of that wire type might be. I think I need to carry 50 mA, with an occasional peak of 100 mA (best guess at this point). I am thinking that 10-12 inches is the length needed.

Looking some more on eBay (and trying different search terms), I found a few sellers who offer 1.0 mm pitch ribbon cable. This is very likely to be something that was designed for board-to-board jumpers, where many parallel signals were needed in a confined space. If the telephone cord does not work out, I may have to try one of those.