RP-SMA PDF has the gender wrong !

Regarding the RP-SMA “FEMALE” PDF drawing on page http://www.sparkfun.com/commerce/produc … cts_id=592 :

It seems like every manufacturer in mainland China is gender-confused when it comes to RP-SMA connectors. The Western rule for determining the gender of a connector is: 1) If the center contact is a hole (a “jack”) then the gender of the connector is “FEMALE” REGARDLESS of the gender of the outside shell. 2) If the center contact is a pin ( a “plug”) then the gender of the connector is “MALE” REGARDLESS of the gender of the outside shell.

Every connector manufacturer in the Western hemisphere follows these rules. It’s simple: If you can figure out what is your own gender then you can figure out what gender a connector is. Apparently, the mainland Chinese have been brainwashed in regards to what determines gender. Perhaps Taiwan should re-educate the mainland.

So, the SMA and RP-SMA gender line-up is this :

SMA, in General: Center contact gender is OPPOSITE of the shell gender.

SMA-M Male center contact with a female outside shell;

SMA-F Female center contact wit a male outside shell;

RP-SMA, in General: Center contact gender is the SAME as the shell gender.

RP-SMA-M Male center contact with a MALE outside shell;

RP-SMA-F Female center contact wit a FEMALE outside shell;

The OUTSIDE SHELL is “Reversed”, NOT the center contact.

This is not hard to understand. The mainland “just doesn’t get it”. Note that the PDF drawing was from a Chinese company. Neither the central contact or the outer shell is “female”, but the description says “SMA FEMALE RP”. All the Western connector manufacturers follow the rules-of-thumb above.

it’s evermore confusing.

Here’s a convenient referene

http://www.l-com.com/familylist.aspx?id=152

and

http://www.l-com.com/productfinder/find … inderID=13

As I understand, some dolt consultant to the US FCC, way back in the 80’s told the FCC they should require odd connectors to prevent or discourage consumers of unlicensed band (pre-WiFi) from using gain antennas that may exacerbate interference issues in low power products. Of course, in quick order, manufacturers produced RP plugs/jacks/antennas. What a waste of money.