Dear friends, I would appreciate a manual to be able to connect the RTK EXPRESS via bluetooth with the Survey Master application, which is free, I have tried to configure it but I have not been able to obtain a location in the application. It does recognize the equipment and makes the connection without problems but it does not give me the location.
configure nmea messages from the menu and if you use for example 4 hz set all nmea messages to 4, save the settings, and after restarting you should see in the surveymaster after setting to Connection device model on Nmea and logging in to gps correctly all needs , 2. from the rover menu make a connection for Ntrip (select Cors) and from my observations it is possible with some Private Ntrip Services to go with others not. success
I am a ZED F9P user and have tried to get fixes via NTRIP in Survey Master 2.9 to no avail. The fact is that I can successfully connect by NMEA to the receiver and to the NTRIP server (client), but the corrections do not arrive and always the receiver stays in “Single”. In the Sparkfun tutorial to work with SURVEY MASTER, the connection to the server is made via CASTER NTRIP and I use an NTRIP CLIENT account. Questions:
Is this the reason why the corrections do not arrive?
Has anyone successfully used NTRIP CLIENT to get fixes?