My new RTK Express is having issues.
Power button is inconsistent. Sometimes turns on when I press the button, usually doesn’t. Sometimes will turn on when I let go of button. Sometimes turns on a few seconds (maybe up to 10?) after pressing.
When it does starts up (randomly, my best success is double clicking the power button, it usually starts up a few seconds later) I get the splash screen with firmware v1.7, then a screen that says, Rover Started, then a flash of the status screen, then Shutting Down… Sometimes it turns on and goes through this process without pressing the power button at all.
I tried a force SD card firmware update. With the SD card in it flashes Forced Update, Rover Started, Shutting Down…
When I received it the battery was loose in the case (came unstuck from the tape). I did open it up to secure it back down.
I’d welcome any ideas here…