I received a Facet Mosaic 10 days ago. The delivery was prompt and safe, but there are problems with the equipment.
The Facet Mosaic rarely starts in the 3-4 seconds specified on the web site. Sometimes the button must be held down for 20 seconds, and even then the Facet starts only after 4-5 quick button-presses in succession. The Facet possibly started (once) showing the information that the web manual says should appear at startup, but since then, that screen is seldom seen, sometimes flashing by when trying to select an option on the “menu”. At startup the Facet immediately enters BaseCast mode, which can’t be changed. A “menu” list comes up if the power button is pressed at just the right m,oment, but the menu doesn’t do anything. Once an option has been selected by toggling through the list, there’s no way to confirm or turn on that selection. After a few seconds the Facet returns to BaseCast operation.
Perhaps the Facet can be configured to a different mode in rxTools. My original hope waqs that I could record a *.sbf file for post-processing, while seeing the survey track on a tablet. Unfortunately, rxToolsv25 isn’t compatible with Windows 7, my main OS (“The procedure entry point CreateEventW could not be locatetd in the dll api-win-core-sunch 1-2-0.dll”).
Fortunately, I was able to find rxToolsv21 on line, and the information said that it works on Windows 7 computers. Unfortunately, the drivers it installs don’t work. I’ve tried manually updating them in the Windows system, but they still don’t transform a USB port into two COM ports. I’ve tried to use the drivers that are linked from your website, but the Windows file is just an executable, without an *.inf file, and simply running it in a terminal window doesn’t enable the transformation.
There are also prooblems connecting the Facet Mosaic to data loggers via Bluetooth. It doesn’t work. I can make Bluetooth connections to other peripherals from a mobile phone and a tablet, but not to the Facet Mosaic. The Facet appears in the list of possible peripherals, so it is putting out a signal, and sometimes a connection seems to be made, but the connection is dropped after a few seconds. This is true whether trying to connect in SW Maps, in Qfield or in the configuration screen. Connection also drops if a wired, serial connection between SW Maps and the Facet Mosaic is tried.
To sum up: The Facet Mosaic does not consistently turn on in a predictable manner. The Facet Mosaic does not communicate with outside data loggers via Bluetooth. The Facet Mosaic cannot communicate to a computer via cable. Without a connection to a computer I can’t configure the Facet nor even determine if it is receiving satellite signals.
Perhaps there’s a firmware fix for these problems, but I would have expected that the latest firmware was installed before it was shipped to me. If there’s not a fix that I can perform, I’d like to return the product and get a refund. Let me know if I need an RMA number.