Rtk surveyor configuration without wifi

My Rtk surveyor stopped sending out a Wi-Fi signal. Is there another way to configure the setup of the receiver? I have the latest Rtk surveyor firmware update Sept8th 2023 and the latest zedf9 firmware 1.32.

Is there another way to configure the setup of the receiver?

Yes. I prefer serial but there are multiple interfaces. Please see docs here: https://docs.sparkfun.com/SparkFun_RTK_ … th_serial/

Thank you. I downloaded Tera Term and changed to correct baud rate and set local echo on. It seems the surveyor and is displaying GNGSA and other data streams but when I hit a key doesn’t default to the system page. Any idea what am doing or not doing correctly?

Be sure you are plugged into the connector marked ‘ESP32 CONFIG’.

Thank you. Any idea if I can stream Bluetooth data (Rtk corrected data) to u-center or another program simultaneously to collect data and assess position drift in real time? U- center blanks out the COM port of the receiver when hooked up to the UBox config port of Rtk surveyor when sending Bluetooth data to a smart phone.

I think STRSVR can be used to listen to one serial pipe and distribute/copy that data to multiple endpoints.

If you’re not familiar with RTKLIB, and you’re on Windows, I recommend rtklibexplorer’s fork: https://github.com/rtklibexplorer/RTKLIB/releases