Good evening (or morning in Amman),
I have incorporated a servo into a project for my 1959 Impala and am getting some “bounce” at the end of each cycle. The idea is to press a (locking) button which will activate a set of relays and a geared motor (with position sensor) and a servo. The geared motor will rotate the license plate down to expose a rear view camera and the servo motor will rotate the (former) ashtray to expose the display to view what the camera is “seeing”. There is also a separate button to activate the license plate to expose the gas tank filler (no issues with this circuit). However, when I activate the “camera” button, both mechanisms activate but the servo bounces at then end of the cycle and basically opens and closes a few times before finally opening. The same happens when closing. I have diodes everywhere but that does not seem to help. I put the SparkFun servo trigger on it’s own power supply and that seemed to do the trick but that is not a real world solution (as everything will be on the 12vdc car power).
I am using this for the geared motor:
https://www.amazon.com/gp/product/B07GD … UTF8&psc=1
(I wold be happy to use a servo but am not sure there is one available to handle the required torque to rotate the license plate AND can be controlled by the SparkFun servo trigger). I will look into using a servo for this once I finish the fabrication but living in Amman, Jordan I do not have access to the machines I would in the US.
For the ashtray, I have a SparkFun generic high torque servo and a SparkFun servo trigger.
I have attached the TinyCAD circuit I designed using relays. I would attach a video but am not sure what file types are allowed.
So my questions are:
What is causing the bounce and how do I get rid of it?
Could I do all of this with an Arduino logic circuit? I am a mechanical engineer and NOT a programmer so the coding will take me some time to learn.
Thanks!