Single Command over Serial Interface to export or print out to screen ALL settings, all Firmware versions of all components?

I am just about 100% on my new RTK Torch, and want to document my journey and the settings that are working for me for all the equipment involved. Is there a Serial Port command that will list out all current settings?
And the Firmware in use by each of the modules in the RTK Torch?

If you have an SD card inserted it should auto-save all settings onto the card

You can then open it in a text editor, print (after disconnecting, rmeoving SD card and putting it into a reader)…as far as I can tell Configure with Settings File - SparkFun RTK Product Manual

I don’t see a memory card anywhere on the. RTK Torch. I think the Facets have memory card slots but the TORCH does not??

I guess I could step thru all the settings via serial port one by one but it is a messy output but on the upside it would show rookie users like myself each command to get each setting.

Chris

Ah, apologies - Somehow I got it mixed up with a facet

You’re right, It looks like the Torch doesn’t support that :+/ Configure with Settings File - SparkFun RTK Everywhere Product Manual

Maybe make a screen recording or screenshots of the menus using rtk.local?