Here’s my configuration:
“Venus GPS Logger with SMA Connector” attached to the “Breakout Board for FT232RL USB to Serial”
I have the Skytraq GPS software 0.5.050 running on my Macbook Air under Windows 7 (via Bootcamp).
The Skytraq sw seems to be reading the Venus GPS logger just fine. I also seem to be able to create a log. However, when I select “Log Read Batch” it creates a Data file which looks like binary data. Choosing “Log Decompress” doesn’t seem to make any difference.
I’m a Mac user, so I can’t figure out if this is a Windows issue or a Skytraq issues.
Also, there is amazingly NO documentation I can find on the Skytraq software.
Suggestions?
Rasjad