I’m working with the SM130 RFID Chip and am running into a peculiar problem I’d like to try to resolve.
If the arduino and antenna start up while a tag is already on the antenna, the reader has no idea that a tag is sitting there. It won’t notice until I remove the tag, at which point I can get the chip to realize that the chip is gone.
I’ve tried toggling the antenna power on/off to see if that helps with sensing the tag’s presence, but to no avail. Does anyone have suggestions for how to resolve this?
Aaand it turns out that turning the antenna on/off before selecting a tag fixed the problem. My first attempt at implementing it just didn’t work right… but it’s fixed now!
Quick question. I’m trying to use your library, but when I try to compile your example, I get the following
This report would have more information with
"Show verbose output during compilation"
enabled in File > Preferences.
Arduino: 1.0.5-r2 (Windows NT (unknown)), Board: "Arduino Uno"
read_tags.ino: In function 'void setup()':
read_tags:11: error: 'class SM130' has no member named 'connect'
read_tags.ino: In function 'void loop()':
read_tags:15: error: 'class SM130' has no member named 'seek_tag'
read_tags:17: error: 'class SM130' has no member named 'parse_response'
read_tags:18: error: 'class SM130' has no member named 'set_flag'
read_tags:19: error: 'class SM130' has no member named 'print_serial'
Any idea why this isn’t working for me? Thanks for any help.