Hello, I’m looking for a cost-effective way to measure a gap with + or - .5mm precision, I would need 4-corner measurements, ( 4-sensors) and I can mount the sensors at a minimum distance of about 5mm, with a max. distance of150mm. Each sensor would need individual read-out for adjustment. Any voltage could be accommodated. The surface of the object being gap measured is an aluminum panel with nickel coating. Thank you for any advice and help. AH
Welcome @JD2025R !
I have some experience with structural deformation monitoring, but it might not apply to your application.
We sometimes used a Linear Potentiometer as a voltage divider that provided great resolution. The problem is gaps don’t always behave in 1 perfect direction (for the rigid mounted linear pot).
Ended up with 2-peice “visual” crack monitors that you can also use digital calipers to resolve to about 0.25mm effectivly. Below is a relative example:
What is the overall range you need to measure, and is the direction defined and stable for each location ?
Hello Ryan, thank you for responding to my post. I should have given more of an explanation, but I didn’t want to get too wordy as this was my first post and I’m not sure of the rules. Here is what I’m trying to do, we have several rotating print presses, ( carousel ) machines. It is critical that the pallets are all level and on the exact same plane as all pallets, (8 total). Typically, I have been leveling the pallets with a couple of machine mounted dial indicators. The problem with this process is that I need to manually lift the dial indicator pin and rotate the machine for the subsequent pallet, each time I do this the dial indicator is moved slightly, and I end up with poor measurements. I would like to mount 4 individual measuring devices at all 4 corners of the pallets on a floor mounted stand and not have to touch or move the measuring devices as I rotate the machine for the next pallet. This would eliminate any movement of the instrument giving me a quicker and more accurate means of leveling the pallets. The gap could be as close as a couple of mm, as it stands the pallets are typically all within a mm of each other, I would like to get to .5 mm on all sides. I tried doing a Google search and the SparkFun site came up. Thanks again for any advice and or help. Alan
Alan, thanks for the extra info…much different project than what I originally guessed.
To my knowledge, Acuity Lasers are the “go-to”, such as the AR100 or AR200.
I don’t think the typical ToF sensors at SparkFun will work for you, but I could be mistaken.
Maybe others will chime-in with the additional info you provided.
We don’t sell anything with that spec; as rftop said a laser is probably the standard method (pricey though!)
I have seen folks use something like a photocell and a small aperture to detect alignment (mounting needs to be very accurate…use backlight to adjust and epoxy in-place)
I also saw a video where someone opened up a digital caliper and was able to get its reading/output via serial if your project lends itself to such (Mitutoyo are a great brand) instead. 4x (or more) shouldn’t be too hard on an MCU with lots of I/O
Thanks for the info, have a great day Alan
Thanks Ryan, I appreciate your willingness to help. Have a great day. Alan
Thank you for the responds, I will continue my quest. I appreciate the input, I will keep you posted if I come up with any new ideas.
Thank you rftop for the input, I appreciate any help I can get.