having trouble with wav trigger board- for the first ever I do not want it to be polyphonic but… I can’t seem to save the
stop latch or anything other than polyphonic play back. I have tried with just deselecting it but that doesn’t seem to work either…trying a new card and different board now as my last hope. Please do you have any suggestions- desperately need to get working properly for an artwork that won’t play tracks over one another
Type: This option affects only certain trigger functions. For the “Normal” trigger function, “Edge Triggered” starts the track when the trigger first goes active, and the track continues to play until stopped by some other event. “Level Triggered” starts the track when the trigger goes active, but the track plays only as long as the trigger remains active. When combined with the “Stop” function, “Level Triggered” will prevent one or more tracks from starting as long as it remains active, creating an “inhibit” function. Beginning with firmware v1.20, “Latched” will activate on a transition but remain active as if it was level type. Another trigger is required to stop any action that is started by a “Latched” type trigger.