I have been working with the Sparkfun RTK Facet L-Band GPS and it has been great getting fixed coordinates while dynamically moving. The problem I am having right now is that when the GPS is sitting on a table, I can see the reported position drifting significantly (3ft+) over 7-10 seconds. The GPS is in fixed mode and it also has 20 satellites in view.
Two things I have tried are:
setting an atmospheric mask so that it ignores satellites up to 20 degrees above the horizon
setting a static hold minimum speed which works to hold the position but when actually moving, it creates a new issue of inaccurate position reporting
Are there any other settings that I can tweak in order to have the L-Band GPS stop drifting.
The problem I am having right now is that when the GPS is sitting on a table, I can see the reported position drifting significantly (3ft+) over 7-10 seconds. The GPS is in fixed mode and it also has 20 satellites in view.
Are you indoors? If yes, you’ll have considerable degradation in your position information. 3+ feet (1m) is considered good for an occluded view.
While 20 satellites sounds good, you should see 30 or more. 20 tells me you may have an obstructed view of the sky. An RTK fix (0.01 to 0.1m accuracy) requires a clear view of the sky, whereas a regular fix can be obtained near windows or in dense foliage but the accuracy will only be 0.3 to 1m.