I need technical support for the Thing Plus Matter kit that I purchased from the Sparkfun shop. Currently, I am experiencing an issue where Simplicity Studio only detects the J-link but is unable to detect the MGM240P chip (it doesn’t show Sparkfun Thing Plus MGM240P). The Simplicity Studio version I am using is SV5.7.0.2, Gecko SDK Suite v4.3.0.
I kindly request your assistance in resolving this issue.
Be sure to hit the rest button and see if that helps. Next I would say try starting over (uninstal, etc); did you use the auto-or manual install the 1st time? It looks like it should should initially appear as a J-Link https://learn.sparkfun.com/tutorials/sp … ware-setup and then appear as the sparkfun board afterward
I tried press the reset button , uninstalled SS5, but the issue persists. Only the J-Link is being recognized, and the SparkFun board isn’t appearing. I purchased 3 kits, and 2 of them are working fine. However, one kit is experiencing this problem.