Unable to connect to Sparkfun Thing Plus Matter

I recently purchased a Sparkfun Thing Plus Matter to use instead of an Arduino Nano and I’m having trouble connecting to it via USB-C. In the Arduino IDE I installed the appropriate board from the board manager, but when I try to upload a sketch I get this error:

ERROR: Could not determine the JLink serial number of the device corresponding to serial port 'COM4', which reports serial number ''. DONE Failed uploading: uploading error: exit status 0xffffffff

From the github associated with the board, the instructions say I need to burn the bootloader first. Doing that, I get the same error as above. In the github instructions, it says “If you have trouble with flashing you may need to install the J-Link USB drivers - it’s part of the J-Link Software and Documentation pack”. So I followed that installation and restarted my computer, but nothing changed.

I also followed the Sparkfun hookup guide which says to use the Simplicity IDE. According to those instructions, the board should be automatically recognized when it is plugged in, but the IDE never recognizes the board.

Searching directly for the error from the Arduino IDE also hasn’t given me a lot of results to go on either.

Could this be an issue with the specific board that I received? Or am I missing something else about the installation and setup? This is my first time using a non-Arduino microcontroller and I’m not sure if it’s user error or not.

I honestly have only dealt with a J-link once, so I’m no expert…but the let’s make sure the board is alive

Before flashing, plug the board into USB-C and:

  • See if any COM port appears
  • Check Device Manager → do you see “Unknown Device” or nothing at all?
  • If absolutely no USB enumeration happens, then the bootloader is definitely missing or corrupted.

Been a while since I looked at this board, but I believe this problem happens if the debugger chip on the board has a problem.

One problem that I did see once was that this diode broke off, which then put the debugger chip into sleep mode. Can you please check whether it’s present on your board?

If that’s not it, there’s a number of other things it could be. But given nothing you tried worked (all of it should have), I suspect there’s a defect with your board.