Hello, I had a question regarding the data sheet for the TAL220 10kg straight bar load cell. The data sheet says that it is rated at 1 mV/V. I wanted to clarify that this rating is for when the load cell is under the maximum rated load of 10kg? So, hypothetically, if I loaded 10kg onto this load cell with 5 Volts, I would get a reading of 5 mV, correct? Thank you for your help!
Yes, the load cell’s full scale output at capacity is approximately [rated response]x[excitation voltage].