Hi,
What’s the easiest way to track time on the logomatic v2 ?
I don’t need time since EPOCH, (that would be nice) but just how much time has elapsed since the last time a record was written.
Thanks
H
Hi,
What’s the easiest way to track time on the logomatic v2 ?
I don’t need time since EPOCH, (that would be nice) but just how much time has elapsed since the last time a record was written.
Thanks
H
I’m batting 0 for 3 on these forums. ![]()
Ok here is a reply to my own question. You do it like this:
//Set the time
void set_time(void)
{
PCONP |= (1<<9); //Ensure RTC is powered
CCR = 0x12; //disable RTC, set xtal flag true
//update time registers
YEAR = 2009;
MONTH = 12;
DOM = 30;
HOUR = 22;
MIN = 43;
SEC = 0;
CCR = 0x11; //enable RTC, keep xtal flag true
char debug[128];
sprintf(debug, “YEAR: %d MONTH: %d DAY: %d HOUR: %d MIN: %d SEC: %d\r\n”, YEAR, MONTH, DOM, HOUR, MIN, SEC);
}
I also found the docs for the chip:
http://www.nxp.com/documents/user_manual/UM10139.pdf
J
Hello! I would like to add a time stamp to each voltage reading recorded by the Logomatic v2 as you did. I am familiar with code, but not experienced enough to edit pre-existing code. Where do you add the code into the main.c file of the logomatic’s firmware. Do you have to edit anything else? I am very noobish when it comes to programming. Thanks.