Ok, there are a few different modchips out there you can make for the wii, but I am interested in making the wiikey. I am having issues designing this thing though. I am a beginner at designing PCB’s so any help would be greatly appreciated. It uses just a basic Atmega8L, a couple of capacitors(not sure what size, but I believe they are 0.10µF) and a resistor(1k Ohms). I have some pictures of the boaerd I want to design, but I just do not know how to design some of the sections. Like the big chunk of copper under the Atmega8L(I believe that is called a copper pour). I also don’t know how to use the back side of the board to make a ground plane and stuff. Also, the pads near the cutout that get soldered to the Wii board, they are colored like green, blue, yellow, cyan. Or the other holes with the pads next to them for GND and VCC
Anyways, I guess what i am asking is, if I upload the pictures of the board I am trying to make, and the schematic and board that I have already tried to make, can you guys help point me in the right direction? Thanks in advance for any help you guys give out.
P.S.
If this is in the wrong section, could a Mod please move it to the correct one?
http://img2.putfile.com/main/6/16502014227.jpg
http://img2.putfile.com/main/6/16502014249.jpg
http://img2.putfile.com/main/6/16502014224.jpg