Hello, i have a wav trigger interfaced to a pinball machine to replace a crappy sound card that someone replaced the chimes with. I have relays that trigger the wav card in place of the original solenoids. Everything works great. I am trying to trigger input 15 to play one of 3 tracks randomly and input 16 to stop. These tracks are 100-102. I cannot get this to work. Is it even possible? I have installed the latest firmware. When i short input 15, nothing happens. I know the wav files are ok as i had them set up on triggers 9,10,11. I could not get them to latch. I would like to use these 3 files as background music.
Thank you