Wav trigger random play

Hello, i have a wav trigger interfaced to a pinball machine to replace a crappy sound card that someone replaced the chimes with. I have relays that trigger the wav card in place of the original solenoids. Everything works great. I am trying to trigger input 15 to play one of 3 tracks randomly and input 16 to stop. These tracks are 100-102. I cannot get this to work. Is it even possible? I have installed the latest firmware. When i short input 15, nothing happens. I know the wav files are ok as i had them set up on triggers 9,10,11. I could not get them to latch. I would like to use these 3 files as background music.

Thank you

Albert

Try to enable polyphony and perhaps ensure the non-default track names are being looked up/triggered properly http://robertsonics.com/wav-trigger-onl … /#chapter8

It also might help (unsure how the random function is coded) but only having 3 tracks for a random selector (guide states it will never replay the one it just played before…) only having 3 might be confusing it - try with 5 or so? You could always copy and give give them new names (pick from 6 filenames, but really it’s 3 tracks twice)

I have tried adding wav files. It seems that if i use input 15 as my trigger it will not play anything but track 15 even with trigger 15 set as contact closure, edge, random. Track range 100-104. It plays track 15 once then stops. In have retrigger checked, polyphonic and loop selected.

I have input 16 set as contact closure , edge , stop , track range 15-105. I have tracks 15, 101-105. This does not stop the track from playing