hi there!
small problem.
i want to use the WAV trigger for something that seems simple enough: press a button, hear a single random soundfile.
only when that file has ended, the WAVtrigger should respond to a new button press to play another file.
while the file is playing, i want button presses to be ignored.
now i have hooked up a button to trigger 1.
my settings are: Trigger01, contact closure, edge type, random (tried ‘next’ as well.).
non-inverted, re-trigger disabled (want files to play all the way through), polyphonic disabled (want to hear only one file at a time), loop off.
if i press the button multiple times but rather slowly, all seems well.
however when i press the same button in rapid succession, files don’t play all the way through and at some point a new file will start, interrupting the one playing. after that, the WAVtrigger seems to go haywire in whether it will respond to a retrigger or not. even slower presses will retrigger.
i tried upgrading to both firmwares 130b and 131, as for 130b it states ‘Fixed bug that allowed track re-trigger if both Re-Trigger and Poly options were deselected’, which describes exactly what is happening.
i upgraded using the sparkfun FTDI (and the flasher app says upgrading is successful). no luck, same behaviour.
i could insert a 555 timer to slow triggering down, or i could run trigger + PLO signal through an AND gate, but i would think the WAV trigger should be able to do what i want on it’s own?
any experiences with this? thanks!