I’m running an RN-XV module with version 2.38 firmware. The boot message says:
WiFly Ver 2.38, 12-11-2012 on RN-171
I have got the module configured and it automatically connects to my wifi network. I have a CP2102 USB-Serial adapter connected to the RN-XV’s serial ports and 0V. I am feeding 3.2V in to the RN-XV Vdd pin from a bench power supply.
I have noticed that when I pull power off the RN-XV and re-apply it, the device fails to start. I don’t mean it won’t connect, it literally doesn’t start up. Even leaving power off for some minutes and re-applying it, won’t restart the module.
Is this a problem with the module’s hardware implementation? Or is there a sleep mode kicking in that I haven’t found out about yet? Any information or pointers would be great.