WIG-13660 No sound/Not Triggering

Hi I just bought a WIG-13660 wav trigger board - it powers up but when pressing the trigger button nothing happens - I have the 001.wav file on the SD card - i have also tried added the init file (although not sure if done correctly). Still nothing - when power on it flashing about 5 times - then just blinks every second.

Please help - This is for my halloween haunt which is about a week away DOH

Hi fcig2000 and Sparkfun.

I have exactly the same problem over here.

Not sure if it’s the micro SD card that needs to be a specific model for the board or specific formating. I made it FAT 32. Named my WAV 001.wav as well. Plugged headphones in jack, put a button in T1 and grnd and try the trigger button as well. Nothing works.

Please help somebody.

https://robertsonics.com/wav-trigger-online-user-guide/ run through this guide and/or the troubleshooting steps mentioned near the end and see how that goes

I found out that I was using a 64GIG - I replaced it with 32 and works fine. On the other hand my other wav trigger- triggers but no sound from the output