Windows 10 does not recognize USB connection to DNSS FLEX breakout

Tested USB C cable, freshly installed Windows 10, CH342SER installed, Firewall disabled, USB connected direct to motherboard.

Sparkfun quickly replaced the first GNSS breakout board, neither board is recognized. A noname Arduino using CH340 chip is recognized.

I am either unlucky or I am frying boards?

Any ideas?

Hi @malcox0 ,

Please check that you are connecting to the UART port, not the USB port.

I hope this helps,
Paul

It certainly helps. I am confused, can you explain why I should connect the USB to the UART socket instead of the USB socket, not intuitive. What is the USB connector for?

Is there a paragraph in the docs I have overlooked?

Malcolm

Hi Malcolm (@malcox0 ),

Please check the docs link below. If the docs need to be improved, please let us know.

The “USB” connector provides a direct connection on GNSS modules that support USB: mosaic and ZED.

The “UART” connector provides access to GNSS UART1 and UART2 via a CH342 interface.

I hope this helps,
Paul

It’s in the features and specs section on the product page:

USB USB-C connector
Provides a direct pass-through connection to the attached module’s native USB interface (requires a USB-capable GNSS module)

UART USB-C connector
Interfaces to UART1 and UART2 on the GNSS Flex Module via a CH342 interface