It looks easy. Put the pins in place, close the connector, voila!!!
But I can’t close the connector at all. So I try using pliers. Still really hard!!! but finally it clamps down, and the connector closes. Pick it up, and the fsr just falls out!
It’s been made clear I can’t return it now.
Has someone used this succesfully in this application? I did buy two (but that’s because I have 2 ribbons…) so I can try again.
I did clip the leads. Somehow I missed the video on the product page. The video does not do a good job of showing it, but at least I realized I needed to do it.
But I’ve mangled all 4 of my amphenol connectors without getting a good connection. I got one that looked good (although the plastic part wouldn’t lock even then) but it was shorted out. It does seem, looking closely, that the terminals are slightly off center on the ribbon, so maybe that’s why.
Any other suggestions for attaching it? Now that I’ve clipped the leads I can’t use a screw terminal
The fsr itself does still work, using alligator clips. I guess I could buy another round of connectors and keep trying, as they don’t seem to have injured the ribbon.
I used a two-pin screw terminal on my other ribbon, and it worked great. I’d certainly recommend that over the amphenol.
It is difficult to see the actual leads of the FSR from that photo. Can you try removing them from the clincher connector and take a photo of the bare leads? Like I mentioned in my reply on the other user’s topic about these same connectors, it may work to carefully solder to the leads on your FSR. You could pre-tin wire, solder it into place quickly (taking care to not leave your iron on the lead for longer than a few seconds) and then you could run the wires to screw terminals or another connector of your choice.
okay, yeah, I may try that with your encouragement. I am pretty good at soldering these days, and I think I can do it quickly enough… worst case, I’m out $20…
thanks!
You’re welcome! Pre-tinning the wires will really help out here to reduce the time you’ll have to have the iron touching the leads on the FSR. If you have some water-soluble flux like [this, that will also help the solder melt and bond quickly to the leads and wire.](Chip Quik No-Clean Flux Pen - 10mL - TOL-14579 - SparkFun Electronics)