External power button error, charge led failure and no Wi-Fi connection in RTK Facet.

Good afternoon

I have a problem with the GPS RTK Facet, First the LED has a false one since sometimes it lights up and in others it doesn’t, I thought that the card had a fault or something, then when I followed the manual for disassembling and assembling the GPS, the external button ignition no longer works; However, the internal one has no problem.

The LED continues to present the error, I thought it could be the version, however I put the ZEP-F9P HPG 1.32 firmware_120522.bin version on it and updated it to the firmware version v3_0.

About WIFI, the RTK Config network does not appear on any device and in the terminal it seems to be on.

the external button ignition no longer works

Be sure to seat and reseat the overlay tab into the display board.

The LED continues to present the error,

The charge LED should turn on when charging and off when fully charged. It does not rely on any firmware. Changing the firmware on the ZED or the ESP will have no effect on the LED.

About WIFI, the RTK Config network does not appear on any device and in the terminal it seems to be on.

Once the device has entered WiFi AP mode (https://docs.sparkfun.com/SparkFun_RTK_ … plus-facet) you should be able to connect to the WiFi network ‘RTK Config’ from your phone or desktop computer.

If you continue to have problems, feel free to return the unit for inspection. https://www.sparkfun.com/returns We can normally get a unit shipped back to a customer within 48 hours.