Firmware update ZED-F9P (Qwiic version) via the ESP32 WROOM module using the Qwiic (I2C) connection

We currently utilize a significant number of your ZED-F9P (Qwiic version) and these are connected via the ZED-F9P Qwiic to the ESP32 WROOM.

Is it possible to update the ZED-F9P firmware via the ESP32 WROOM module using Bluetooth, and using the Qwiic (I2C) connection? Or is this process strictly limited to the USB-C interface? Please note that on all our ZED-F9P units, we have disabled all connections except for I2C and USB.

Thanks in advance for your responses

Hi @Jan-Henk ,

Yes, it takes a little work, but it is possible. Please see the post linked below. That post is about upgrading the X20P via I2C, but the same is possible on the ZED-F9P.

Best wishes,
Paul