How do I terminate the wires for this Android device?

Please see this image: http://i.imgur.com/8EezOky.png

I received this device and the following specification from the manufacturer:

"Power Supplier 18-36VDC

Power Consumption =< 25W

What component do I need to use to terminate these copper wires so I can power this device?

Use whatever matches the connector on your power supply. It can be anything from soldered connections, wire nuts, or mating jack.

If you need a power supply, I would grab an old laptop brick (most are 19V) or 24V wall wart. The device needs 1.4A minimum current at 18V (the supply can provide more…)

/mike

I purchased this: https://www.amazon.com/dp/B00ZBCLJSY/

Am I correct in that this can power on my device?

That should work fine.