Greetings,
I bought this kit (NVIDIA Jetson Nano Developer Kit (V3) DEV-16271), and I have been trying to set it up using the SD Card Image download, following the headless setup methods that are posted in various places on the Internet. I don’t have an HDMI display to try the GUI setup. I first tried it many times with a Linux laptop and “screen” app, then more times with a Windows 7 computer and Putty. In each case I start with s freshly burned SD card image, following the Nvidea instructions for each system (with Linux you simply use Etcher, with Windows you first format the card with SD Card Formatter.)
Every time, the following sequence happens: When I plug in the power supply (5V 4A supply that came with kit), I see the green LED on the carrier board come on & stay on the whole time, but NOTHING ever happens in the window of the host computer. I’ve tried everything from doing nothing to hitting “Space” as per one set of instructions, “Escape” per another set, “Enter,” Control-A followed by other chars (in Screen) and all sorts of things. I have waited a long time in each case, but nothing ever appears in the screen window, just a black background with the first character lit where the cursor is.
I’m using the USB cable that came with the kit (that I’ve verified does pass data), Also I’ve got the the USB camera that came wit the kit plugged in, as well as an Ethernet cable.
By the way, the SD card that came from you guys with the kit is a dud, I couldn’t read it or format it on either Linux nor Windows. So, I’m using other SD cards that I had on hand, some were fresh out of the wrapper, others used.
I have used other SD cards that I happened to have around, Samsung high-speed cards (32 GB) that work in my high-end cameras, so I know it’s not a problem with the SD cards. I have also re-downloaded the SD card images (Jet pack 4.5.1).
As far as I can tell, the Nano is simply not booting. I have exhaustively searched the Internet and every forum I can find. The only thing I have found that’s remotely similar was on the Sparkfun forum, e.g.
“NVIDIA JETBOT KIT JETSON NANO LOGO BUT NO BOOT SEQUENCE” seems similar, but since I don’t have an HDMI monitor to hook up, I can’t even verify if the logo is displaying. I am exhausted from doing the same things over & over, read every forum I can find, Googled to exhaustion, I’ve watched every Youtube video I can find that may give any insight…it seems so straightforward, but it’s NOT WORKING… AHHH!
Everyone else seems to be stuck on much more advanced steps, where they’re working on actual apps or experiments–it seems that everyone else gets this part done with no trouble! Why am I having these problems?!
Thanks in advance for any help you can provide.
HELP!