MiniMod No Longer Acquiring Signal within Specs

All of a sudden, it is taking 5 minutes of sitting outside, on a clear day to get a signal that is lost within a minute. Accuracy has also gone out the window (± 1000m off).

I do not believe that I have overpowered it as it hasn’t moved on the breadboard for weeks, but even if I had, I don’t think that would explain this (i.e. broken but still functioning occasionally?).

Any ideas? Anyone else seen this? This is extremely urgent that I get this resolved soon, any help is greatly appreciated, and my head can only stand so much more beatings against the wall.

Power:

5V

45mA

EDIT:

I forgot to mention that it is recognizing only a single satellite, occasionally two. I can read the time and date of fix, but that is it since obviously it can’t calculate position data based on two satellites.

Again, I am going insane with this. Can anyone offer any suggestions to get this thing back up and running again. As far as I can tell, NOTHING is wrong with the board, so I have literally no idea why it won’t find more than a few satellites.

Moving does not change its acquire time. I have walked with it, driven with it, stood still, etc.