Hello.
I used before a GPS6MV2 GPS board which was very imprecise. I used it with a small antenna. But this board allows me to receive uickly some positions for tests purposes.
GPS6MV2 board:
I have buyed a Sparkfun GPS NEO-M9N, with an active antenna, but I have NOT YET a cable between U.FL connector and antenna.
I start then to use the Sparkfun board with my small antenna. But, at the same place of my home, if I receive correctly all GPS frames, I never receive any positions. I have done tests with the u-blox tool “u-center_v21.05”, and it it the same situation : frames, but no positions. Does it can be caused by small quality antenna ?
Sparkfun GPS NEO-M9N with small antenna :
Active antenna :
Sample of received frames :
“$GNGGA,0,00,99.99,*56”,“valid”:true,"
“$GLGSV,1,1,00,1*78”
“$GAGSV,1,1,00,7*73”
“$GNGLL,V,N*7A”
“$GNVTG,N*2E”
“$GNGSA,A,1,99.99,99.99,99.99,1*33”
Best regards.