Postcard Lora base crash

I have successfully fed my facet as a base to my postcard as a rover with Lora radios. Anytime I have the Lora radio connected to the postcard and do base mode it crashes repeatedly. I set the baud rates of both devices to 57600 bps on the radio ports.

I was able to get down to 20 mm on the postcard connected to the base facet.

I turned down a lot of nmea messages and that prevents the crash. So maybe in base mode you have to limit it the amount of traffic being sent out.

That means you need to limit NMEA Messages. You only need to send the essential messages for RTK.

But in base mode nmea shouldn’t really send one would think