QWIIC Adapters for More Pinout Combinations

If anyone is interested, I designed and ordered pc boards from Oshpark.com that allow for more combinations of VCC, GND, SDA, SCL when adding the Qwiic connectors to an existing product with .1" 4 pin headers.

The OLED I was trying to use and add to the Qwiic chain had a different order of pins than the Sparkfun Qwiic Adapter board so I made a board with 4 different combinations. You have to add the Qwiic surface mount 4 pin adapters (JST04) and then choose the correct set of .1" holes that match the IIC port you want to interface.

These boards are public so you can order them yourself.

JST04 from Sparkfun
Qwiic Adapter 1
Qwiic Adapter 2 (90 deg)

This is a really great idea! If I was doing it, I’d try only a single set of 4 pin headers, but make the pin assignments jumper-selectable. You might even get a smaller board that way.